2019-04-17 5:41 PM
Hello,
I am able to compile the M4 examples and it looks as though they run as expected ( I can see the log trace on the A7 side from the linux console). I would like to examine the log trace from the M4 side also as I would like to modify some of these examples for further use. In the OpenAMP_TTY_echo example (main.c) are the following lines
log_info("Cortex-M4 boot successful with STM32Cube FW version: v%ld.%ld.%ld \r\n",
((HAL_GetHalVersion() >> 24) & 0x000000FF),
((HAL_GetHalVersion() >> 16) & 0x000000FF),
((HAL_GetHalVersion() >> 8) & 0x000000FF));
I was curious as to how I can enable these lines. Do I need to enable putc associated with one of the UART instances or ..
Basically just want to know how I can have console functionality on the M4 side also
Thanks
Victor
Solved! Go to Solution.
2019-04-18 12:16 AM
Hello, I'm not 100% sure of the answer,
Need to define __LOG_TRACE_IO_ in M4 preprocessor directives
Traces are then available under Linux using e.g. cat /sys/kernel/debug/remoteproc/remoteproc0/trace0
(see Linux_remoteproc_framework_overview#How_to_trace_and_debug_the_framework)
2019-04-18 12:16 AM
Hello, I'm not 100% sure of the answer,
Need to define __LOG_TRACE_IO_ in M4 preprocessor directives
Traces are then available under Linux using e.g. cat /sys/kernel/debug/remoteproc/remoteproc0/trace0
(see Linux_remoteproc_framework_overview#How_to_trace_and_debug_the_framework)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.