cancel
Showing results for 
Search instead for 
Did you mean: 

browser support on STM32MP25

mdivertie
Associate II

Hi,

 I am currently working on a project that requires us to install a browser on our board. We are using an STM32mp25, which is using the Mickledore image. I am finding that the meta-browser layer is not compatible with Mickledore, and if I'm not mistaken meta-browser only runs on Scarthgap. What I've tried to do is switch my layers to the Scarthgap branch, and unfortunately what I find is that from my conf/local.conf is that the stm32mp25 is not a recognized maching (MACHINE = "stm32pm25"), meaning that the stm32mp25 is not supported on Scarthgap.

 

Has anyone successfully installed a browser on the stm32mp25 (eval board)? Any help would be greatly appreciated!

 

For reference I was following along with this demo https://www.digikey.com/en/maker/projects/intro-to-embedded-linux-part-2-yocto-project/2c08a1ad09d74f20b9844e566d332da4

1 ACCEPTED SOLUTION

Accepted Solutions
Billy OWEN
ST Employee

Hi @mdivertie 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

View solution in original post

10 REPLIES 10
Gregory PLANCHON
ST Employee

Hi @mdivertie,

 

Scarthgap is not yet supported by ST delivery. It's plan on the next DV planned for Q4.

 

regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

How could we support a browser (Chromium/Firefox) in the meantime?

Hi @mdivertie,

 

I think you can refer to this forum post to install a browser on MP15 : https://community.st.com/t5/stm32-mpus-embedded-software/qt-wpe-simple-browser-installation-failed/td-p/703413

 

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @mdivertie,

 

Today, there is no official support of Chromium for STM32MP25. It might append by the end of the year.

Internally, we have tried Qt6 webengine that includes Chromium (meta-qt6 layer). Today, there are some performance limitations (some GPU or HW video acceleration are missing) that can lead to a bad user experience. But in kiosk mode and for specific web sites, browsing can be done correctly.

For additional technical info, please contact STM support.

 

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Billy OWEN
ST Employee

Hi @mdivertie 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

Hi Melody,

Yes, we were able to install a browser on an stm32Mp2. A colleague used this recipe

https://github.com/OSSystems/meta-browser/blob/master/meta-chromium/recipes-browser/chromium/chromium-ozone-wayland_130.0.6723.58.bb

Best,

 Matt

Thank you Matt!

So must build the whole os using Yocto. There isn't a package to install to the existing system, right?

And have u also tried a browser on X11 distro? Thank you!

DMårt
Lead

@Billy OWEN 

@PPAGE.13 

@Gregory PLANCHON 

@melody 

@mdivertie 

I'm very intrested of the status of this thread. Is it working now? Lag free browsing at 1080p at Youtube or other?

I'm building a custom board of STM32MP257FAK3 processor. My goal is to use the MP2 as mini-PC for streaming in 1080p. Youtube/GeForce Now by using Chromium. 

Yes I know that MP2 is not meant to be used as a mini-PC. Even if it could be used as a mini-PC. 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer