cancel
Showing results for 
Search instead for 
Did you mean: 

Boot from emmc fail at ODYSSEY STM32MP157C board

zqizh.1
Associate III

Hi,

I tried to let "en.FLASH-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar_v3.0.0" work on the ODYSSEY STM32MP157C board.

Please advise when will produce error : "

Starting version 244.5+

[  5.236977] blk_update_request: I/O error, dev mmcblk1, sector 173056 op 0x1:(WRITE) flags 0x20800 phys_seg 1 prio class 0

[  5.246675] Buffer I/O error on dev mmcblk1p4, logical block 0, lost sync page write

[  5.254488] EXT4-fs (mmcblk1p4): I/O error while writing superblock

[  5.260725] EXT4-fs (mmcblk1p4): mount failed

[  5.269862] VFS: could not find a valid V7 on mmcblk1p4.

" and how to solve it.

The attachment is the output log.

Thanks,

QiZhang

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
IAbde.1
Associate

Hi QiZhang,

try to reconfigure the booting partition of rootfs by adding the same UUID appearing in the err-log file.

Kind regards

Ibrahim Abdelaty

View solution in original post

2 REPLIES 2
OlivierK
ST Employee

Hi zqizh.1 (Community Member) 

I see this SOM has 2 possible boot, SDcard and emmc. Do you have the same error on both boot image?

As it is a non ST board, I guess you can post your question directly on the forum dedicated to this board. https://forum.seeedstudio.com/

Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
IAbde.1
Associate

Hi QiZhang,

try to reconfigure the booting partition of rootfs by adding the same UUID appearing in the err-log file.

Kind regards

Ibrahim Abdelaty