2021-04-06 2:32 AM
Hello Guys.
I have tried bitbake(st-image-core) after a long time.
But I can't proceed with the following error.
This error is partial, and many of the same errors appear(Attach the error as text).
I don't know how to fix it. I need help.
can't find file to patch at input line 39367
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/plat/st/stm32mp1/sp_min/sp_min-stm32mp1.mk b/plat/st/stm32mp1/sp_min/sp_min-stm32mp1.mk
|index 4188cc58a..2ab8e8d4b 100644
|--- a/plat/st/stm32mp1/sp_min/sp_min-stm32mp1.mk
|+++ b/plat/st/stm32mp1/sp_min/sp_min-stm32mp1.mk
--------------------------
No file to patch. Skipping patch.
2 out of 2 hunks ignored
can't find file to patch at input line 39419
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/plat/st/stm32mp1/sp_min/sp_min_setup.c b/plat/st/stm32mp1/sp_min/sp_min_setup.c
|index e10dfbfc0..f57630604 100644
|--- a/plat/st/stm32mp1/sp_min/sp_min_setup.c
|+++ b/plat/st/stm32mp1/sp_min/sp_min_setup.c
--------------------------
No file to patch. Skipping patch.
8 out of 8 hunks ignored
patching file plat/st/stm32mp1/stm32mp1_boot_device.c
can't find file to patch at input line 40016
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/plat/st/stm32mp1/stm32mp1_context.c b/plat/st/stm32mp1/stm32mp1_context.c
|index cf8a91eb4..e77b8a79f 100644
|--- a/plat/st/stm32mp1/stm32mp1_context.c
|+++ b/plat/st/stm32mp1/stm32mp1_context.c
--------------------------
No file to patch. Skipping patch.
2 out of 2 hunks ignored
can't find file to patch at input line 40434
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/plat/st/stm32mp1/stm32mp1_dbgmcu.c b/plat/st/stm32mp1/stm32mp1_dbgmcu.c
|index d0264968c..b9f94af0a 100644
|--- a/plat/st/stm32mp1/stm32mp1_dbgmcu.c
|+++ b/plat/st/stm32mp1/stm32mp1_dbgmcu.c
--------------------------
No file to patch. Skipping patch.
4 out of 4 hunks ignored
can't find file to patch at input line 40523
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/plat/st/stm32mp1/stm32mp1_def.h b/plat/st/stm32mp1/stm32mp1_def.h
|index a40852bde..d458805a1 100644
|--- a/plat/st/stm32mp1/stm32mp1_def.h
|+++ b/plat/st/stm32mp1/stm32mp1_def.h
--------------------------
No file to patch. Skipping patch.
11 out of 11 hunks ignored
The next patch would delete the file plat/st/stm32mp1/stm32mp1_gic.c,
which does not exist! Applying it anyway.
patching file plat/st/stm32mp1/stm32mp1_gic.c
Hunk #1 FAILED at 1.
1 out of 1 hunk FAILED -- rejects in file plat/st/stm32mp1/stm32mp1_gic.c
can't find file to patch at input line 41110
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/plat/st/stm32mp1/stm32mp1_helper.S b/plat/st/stm32mp1/stm32mp1_helper.S
|index bfcd991a3..b80716253 100644
|--- a/plat/st/stm32mp1/stm32mp1_helper.S
|+++ b/plat/st/stm32mp1/stm32mp1_helper.S
--------------------------
No file to patch. Skipping patch.
6 out of 6 hunks ignored
patching file plat/st/stm32mp1/stm32mp1_low_power.c
can't find file to patch at input line 41731
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/plat/st/stm32mp1/stm32mp1_pm.c b/plat/st/stm32mp1/stm32mp1_pm.c
|index cf9fa8e69..627d209da 100644
|--- a/plat/st/stm32mp1/stm32mp1_pm.c
|+++ b/plat/st/stm32mp1/stm32mp1_pm.c
--------------------------
No file to patch. Skipping patch.
9 out of 9 hunks ignored
patching file plat/st/stm32mp1/stm32mp1_power_config.c
can't find file to patch at input line 42112
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/plat/st/stm32mp1/stm32mp1_private.c b/plat/st/stm32mp1/stm32mp1_private.c
|index e2dcd2af7..b94857bcb 100644
|--- a/plat/st/stm32mp1/stm32mp1_private.c
|+++ b/plat/st/stm32mp1/stm32mp1_private.c
--------------------------
No file to patch. Skipping patch.
14 out of 14 hunks ignored
patching file plat/st/stm32mp1/stm32mp1_scmi.c
can't find file to patch at input line 43427
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/plat/st/stm32mp1/stm32mp1_security.c b/plat/st/stm32mp1/stm32mp1_security.c
|index 61db2e7c7..41762fa6b 100644
|--- a/plat/st/stm32mp1/stm32mp1_security.c
|+++ b/plat/st/stm32mp1/stm32mp1_security.c
--------------------------
No file to patch. Skipping patch.
1 out of 1 hunk ignored
patching file plat/st/stm32mp1/stm32mp1_shared_resources.c
can't find file to patch at input line 44194
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------/home/parksh/STM32MPU_EV1_Workspace/SDK/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1-AMI_EMU01/tmp-glibc/work/stm32mp1_AMI_EMU01-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/log.do_patch.52340
ERROR: Task (/home/parksh/STM32MPU_EV1_Workspace/SDK/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-06-24/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb:do_patch) failed with exit code '1'
|diff --git a/plat/st/stm32mp1/stm32mp1_syscfg.c b/plat/st/stm32mp1/stm32mp1_syscfg.c
|index 2fd06f38a..1585590bc 100644
|--- a/plat/st/stm32mp1/stm32mp1_syscfg.c
|+++ b/plat/st/stm32mp1/stm32mp1_syscfg.c
--------------------------
No file to patch. Skipping patch.
7 out of 7 hunks ignored
patching file plat/st/stm32mp1/stm32mp1_usb_desc.c
can't find file to patch at input line 44785
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/tools/stm32image/stm32image.c b/tools/stm32image/stm32image.c
|index 41024e286..209e0c9d8 100644
|--- a/tools/stm32image/stm32image.c
|+++ b/tools/stm32image/stm32image.c
--------------------------
No file to patch. Skipping patch.
8 out of 8 hunks ignored
Patch 0001-st-update-v2.2-r2.0.0.patch does not apply (enforce with -f)
ERROR: Logfile of failure stored in: /home/parksh/STM32MPU_EV1_Workspace/SDK/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1-AMI_EMU01/tmp-glibc/work/stm32mp1_AMI_EMU01-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/log.do_patch.52340
ERROR: Task (/home/parksh/STM32MPU_EV1_Workspace/SDK/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-06-24/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb:do_patch) failed with exit code '1'
2021-04-09 7:23 AM
Hi @SPark.15 ,
Could you please describe further which Distribution package you are using and all steps you did to build ?
Thanks
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.