cancel
Showing results for 
Search instead for 
Did you mean: 

AN5861 - Power rating for R4 (8R2)

alw
Senior

Is there a recommended minimum SMT package size and power rating for resistor R4 (8R2) please?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

R4 is only connected to GND by Q1 for a very short time, defined by the monoflop U1 with R3/C3, so that the heating of R4 is almost negligible depending on its dimensioning. With the approx. 0.4ms (100k, 5.6nF) from AN5861, a resistor size of 0805 is certainly sufficient.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

R4 is only connected to GND by Q1 for a very short time, defined by the monoflop U1 with R3/C3, so that the heating of R4 is almost negligible depending on its dimensioning. With the approx. 0.4ms (100k, 5.6nF) from AN5861, a resistor size of 0805 is certainly sufficient.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
alw
Senior

Hi Peter,

Thanks very much.

Kind regards,

Al