2023-10-24 11:25 AM
Hello! Is it feasible to start FBSD kernel?
So far I stuck with following error (seems to be from tf-a):
Loading kernel...
/boot/kernel/kernel text=0x1b4 text=0x5ad698 text=0x17e3d0 data=0xa4860 data=0x0+0x20c000 0x4+0x88d70+0x4+0xea43b|
Loading configured modules...
can't find '/etc/hostid'
can't find '/boot/entropy'
Using DTB compiled into kernel.
Kernel entry at 0xc0400200...
Kernel args: (null)
metadata: filename:/boot/kernel/kernel, size=11874740 loadaddr=0xc0400000
ERROR: Illegal access to 0xffff0010:
ERROR: FAIL_ID = 0x4c0
ERROR: Non-Secure
ERROR: Privilege
ERROR: Read
PANIC at PC : 0x2ffc97b1
Exception mode=0x00000016 at: 0x2ffc97b1
I'm sure, that control passes to the kernel _start point.
Any clues?
Solved! Go to Solution.
2023-10-27 12:45 PM
it looks like default page builder code for PA->VA translation, implemented by the kernel conflicts with what mmu tolerates...
/usr/src/sys/arm/arm/locore-v6.S:
/*
* First map the entire 4GB address space as VA=PA. It's mapped as
* normal (cached) memory because it's for things like accessing the
* parameters passed in from the bootloader, which might be at any
* physical address, different for every platform.
*/
mov r1, #0
mov r2, #0
mov r3, #4096
bl build_pagetables
Given my board has 512Mb, this translation region must end at 0xc0000000 + 0x20000000 = 0xe000000...
so, mov r3, #3584 fixes this case and eventually kernel passes into translated address mode..
done.
2023-10-26 2:43 PM
It looks like FreeBSD kernel is not allowed to enable MMU... why?
ASENTRY_NP(init_mmu)
....
/* Enable MMU */
mrc CP15_SCTLR(r0)
orr r0, r0, #CPU_CONTROL_MMU_ENABLE
orr r0, r0, #CPU_CONTROL_V6_EXTPAGE
orr r0, r0, #CPU_CONTROL_TR_ENABLE
orr r0, r0, #CPU_CONTROL_AF_ENABLE
mcr CP15_SCTLR(r0)
DSB
ISB
mcr CP15_TLBIALL /* Flush TLB */
mcr CP15_BPIALL /* Flush Branch predictor */
DSB
ISB
mov pc, lr
END(init_mmu)
So, the line 9 (mcr CP15_SCTLR(r0)) makes tf-a completely unhappy...
Is some specific initialization required?
2023-10-27 12:45 PM
it looks like default page builder code for PA->VA translation, implemented by the kernel conflicts with what mmu tolerates...
/usr/src/sys/arm/arm/locore-v6.S:
/*
* First map the entire 4GB address space as VA=PA. It's mapped as
* normal (cached) memory because it's for things like accessing the
* parameters passed in from the bootloader, which might be at any
* physical address, different for every platform.
*/
mov r1, #0
mov r2, #0
mov r3, #4096
bl build_pagetables
Given my board has 512Mb, this translation region must end at 0xc0000000 + 0x20000000 = 0xe000000...
so, mov r3, #3584 fixes this case and eventually kernel passes into translated address mode..
done.