cancel
Showing results for 
Search instead for 
Did you mean: 

uClinux on STM3220G

tido
Associate II
Posted on August 13, 2013 at 11:22

Hi,

I'm new to the STM3220G-Eval board and want to run uClinux on it. 

Are there any ready to use vendor files for uClinux like Makefile, config.arch, config.uClibc, config.linux-2.4 and so on? 

Or is there a similar controller which can be modified for the STM32F207?

Has someone experience with uClinux on a STM32F2 controller? 

Thanks in advance for every kind of help.

Kind regards

Tido

#stm32 #linux
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on August 13, 2013 at 13:46

http://emcraft.com/index.php/products/234

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
tido
Associate II
Posted on August 14, 2013 at 09:48

Thanks for the quick reply,

I now about that project but I wonder if it is possible to get uClinux running without additional memory? 

Even if it is quite pointless with such a small amount of userspace.

Posted on August 15, 2013 at 01:13

There have been some discussions about foot prints of ucLinux, the latter half of

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/uClinux%20on%20STM32&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=28357

deals with the F4, but it should be salient.

We don't see much ucLinux traffic at this forum

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..