cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 - VBAT characteristics - need clarity

ARama.1
Associate II

Hi,

we're using STM32MP1 for our project. we have connected super cap to VBAT.

our expectation is to have VBAT supply power to RTC *alone*. we dont want RAM content to be retained. so that RTC shall remain powered for long time. currently the VBAT is supplying back up power for both RAM contents & also for RTC, so we're experiencing RTC back up for just 5 hours instead of expected 5 days. Kindly help out.

 

should we use RREN/BREN in this case?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hi @ARama.1 

To explain the result far below your expectations, I think BREN and RREN are set, so you should change SW (TF-A or opTEE) or DT to remove this setting.

According to datasheet, power with LSE+RTC only should be typically 1.25uA at 3V

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here