cancel
Showing results for 
Search instead for 
Did you mean: 

spi Overrun: RX data lost when "spi_sync_transfer" too long in kernel

ABouc.1
Associate

Hi,

I would like to make my STM32MP157 communicate with a FPGA in spi. I need to make long transfer (2-3 Mb) spi to get data acquired by the FPGA. But when I use the "spi_sync_transfer" function in my driver, I get the following kernel message:

#spi_stm32 4000b000.spi: Overrun: RX data lost

#spi0.0: SPI transfer failed: -5

# spi_master spi0: failed to transfer one message from queue

This driver works on an ompa3 platform.

I use a kernel linux 5.10, there is my device tree overlay :

/dts-v1/;
/plugin/;
&spi2 {
	ifsttarhf8ch: ifsttarhf8ch@0 {
		compatible = "ifsttar,ifsttarhf8ch";
		reg = <0>;
		spi-max-frequency = <100000000>;
		interrupt-parent = <&gpioi>;
		interrupts = <9 IRQ_TYPE_EDGE_RISING>; 
	};
};

and my device tree :

#include "stm32mp157.dtsi"
&spi2 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&spi2_pins_mx>;
	pinctrl-1 = <&spi2_sleep_pins_mx>;
	cs-gpios = <&gpiob 9 0>,
			   <&gpioi 1 0>,
			   <&gpiob 8 0> ;
	status = "okay";
 
	spidev2_1: spidev2_1@1{
		compatible = "rohm,dh2228fv";
		spi-max-frequency = <30000000>; 
		reg = <1>;
	};
	spidev2_2: spidev2_2@2{
		compatible = "rohm,dh2228fv";
		spi-max-frequency = <30000000>;
		reg = <2>;
	};
};

In my driver i use this code to read on the FPGA :

temp = CMD_READ(ADDR_BURST_DATA_RX); //fpga registry
transfer[0].tx_buf = &temp;
transfer[0].len = sizeof(temp);
transfer[1].rx_buf = data
transfer[1].len = sizeof(u16)*4095*8 // 4095 data * nb channel (8)
ret = spi_sync_transfer(spiHandler,&transfer[0],2);

Another problem, when I modify the "spi-max-frequency" field in the device tree, the clock frequency does not increase more than 12.5Mhz.

Sincerely

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hi @Arthur Bouché​ ,

I cannot answer for the overrun, maybe have a look to

https://wiki.st.com/stm32mpu/wiki/SPI_overview

https://wiki.st.com/stm32mpu/wiki/SPI_device_tree_configuration

Regarding the SPI frequency limited to 12.5MHz, this is probably because your clock tree define a too low frequency for SPI 'kernel' clock. The Linux driver compute the best he can do using peripheral constrains (e.g. SPI divider is 2, 4, 8 , etc...).

You could check the frequency received by your SPI by looking at spi2_k in clock summary.

See https://wiki.st.com/stm32mpu/wiki/Clock_overview#How_to_monitor_with_debugfs

E.g. In our starter package, on DK2, spi2_k is 11.29 MHz which should allows only up to 5.6MHz.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here