2020-01-30 9:43 AM
I am testing Ethernet on the STM32MP1 (on both the EV1 and DK2 eval boards) and seeing slow link up times when the board is connected to a Gigabit Ethernet switch. Here's an excerpt from the dmesg traces showing link up times of 6-7 seconds:
[ 8.931934] Generic PHY stmmac-0:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=stmmac-0:00, irq=POLL)
[ 8.952777] dwmac4: Master AXI performs any burst length
[ 8.956664] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 8.964160] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 8.972895] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 14.169871] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/txSince my application does not really need Gigabit Ethernet, I tried limiting the speed to 100 Mbps in the device tree, as described here: https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration
However the results are still similar; typical link up times are in the ~6 second range.
Is there any way to shorten the link up times?
BR,
Guillermo
2020-02-21 6:48 AM
Hi @Grodriguez
did you try to use static address to remove DHCP request ?
Olivier
2020-02-24 2:07 AM
Hi Olivier,
Yes, I tested with static address, anyway note that the issue is related to the link time (Ethernet level), not to the IP configuration.
Guillermo
2020-07-17 12:47 PM
2020-07-17 12:48 PM
Sorry I am new to the forum, didn't mean to attach the log, wanted to display:
Starting network: [ 3.327679] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [RTL8211F Gigabit Ethernet]
[ 3.368439] dwmac4: Master AXI performs any burst length
[ 3.375121] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 3.386583] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 3.399417] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 3.409993] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 9.067672] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 9.080502] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready