I am currently working with the Yocto BSP/meta-layer you provide for the Odyssey STM32MP157C board. I am trying to include the following packages in my image:
CORE_IMAGE_EXTRA_INSTALL += "kernel-modules"
CORE_IMAGE_EXTRA_INSTALL += "kernel-devsrc"
CORE_IMAGE_EXTRA_INSTALL += "kernel-dev"
However, these packages are not being recognized or supported in the meta-layer provided. The build either fails or reports that these packages do not exist. I would like to understand whether these components are intentionally excluded from your BSP or if there is an additional layer, configuration, or package feed that I need to enable to use them.I built the image using the github documentation in this link
https://github.com/Seeed-Studio/meta-st-odyssey .
Could you please guide me on how to properly include kernel modules, development sources, and kernel headers/dev packages in the image for this platform?
Any help or documentation reference would be greatly appreciated.