Increasing the rootfs size on a stm32mp157f-dk2
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-23 3:19 AM
Hi,
i´m using a stm32mp157-dk2 and want to increase the size of the rootfs partition to 2GB.
To create the image follwed the instructions from https://wiki.st.com/stm32mpu/index.php/STM32MP1_Distribution_Package#Installing_the_OpenSTLinux_distribution .
Before running the bitbake command changed as suggested in https://community.st.com/s/question/0D53W00000EaFPwSAN/rootfs-size-increasing-on-avenger96
1) /meta-st/meta-st-stm32mp/conf/machine/include/st-nachine-common-stm32mp.inc
IMAGE_ROOTFS_MAXSIZE ?= "2097152"
ROOTFS_PARTITION_SIZE ?= "2097152"
2) /meta-st/meta-st-stm32mp/recipes-devtools/sdcard-raw-tools/sdcard-raw-tools/create_sdcard_from_flashlayout.sh
DEFAULT_RAW_SIZE=4096
DEFAULT_ROOTFS_PARTITION_SIZE=2097152
Then while running the bitbake command an error showed up "The initramfs size 181612 (K) exceeds INITRAMFS_MAXSIZE: 131072 (K) You can set INITRAMFS_MAXSIZE a larger value.... ". To avoid this error i increased INITRAMFS_MAXSIZE to 262144 in layers/openembedded-core/meta/conf/bitbake.conf
After restarting the process with bitbake the following errors showed up:
Please let me know, if i missed some steps to increase the rootfs size or did something fundamentally wrong.
Thanks,
stefan_r
Solved! Go to Solution.
- Labels:
-
STM32MP15 Lines
-
Yocto
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-26 8:25 AM
Hi @stefan_r ,
Your ROOTFS looks still bigger than what you set as max size : 2017660 vs 2097152.
Try to update st-machine-common-stm32mp.inc with :
IMAGE_ROOTFS_MAXSIZE ?= "2017660" or bigger
in this case create_sdcard_from_flashlayout.sh is not called/concerned.
Hope it help
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-26 8:25 AM
Hi @stefan_r ,
Your ROOTFS looks still bigger than what you set as max size : 2017660 vs 2097152.
Try to update st-machine-common-stm32mp.inc with :
IMAGE_ROOTFS_MAXSIZE ?= "2017660" or bigger
in this case create_sdcard_from_flashlayout.sh is not called/concerned.
Hope it help
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-27 12:55 AM
Hi Olivier,
i increased the IMAGE_ROOTFS_MAXSIZE to a value bigger than "2017660" and bitbaked my image with this change.
I tried to do this previously, but that time i also added multiple EXTRA_IMAGE_FEATURES in the local.conf which i seems to have caused the Warning with package uboot (can be seen on the picture above). I think that the reason for this warning also caused, that i couldn´t flash the image successful. After a new try to build openstlinux with a fresh repo, where i only added some packages in the local.conf an increased the rootfs it builds and the image can be flashed successful.
Thanks for your help!
stefan_r