cancel
Showing results for 
Search instead for 
Did you mean: 

How to transfer data from the SRAM to the DDR in a kernel module?

MElha.1
Associate II

Hello,

I am working on a project that acquires ADC readings and saves them into a buffer in the M4 side of STM32mp157 chip on DK2 board, now I need to build a kernel module that copies the saved buffer from the SRAM to DDR on the A7 side when a certain interrupt is triggered.

As I am a beginner in embedded linux world I am wondering about the way to do this, I tried memcpy() at first but errors arise when inserting the module (Can't page virtual address error), I also tried converting the SRAM address from physical to virtual before memcpy() but that didn't work as well.

Is there a direct way to copy data between the memories like memcpy() or do I need to use DMA from the kernel module to copy the data, if the DMA is the way, sharing an example would be great.

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @MElha.1​ 

ST deliver a complete documentation and demo for this use case :

https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_principle

https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
Olivier GALLIEN
ST Employee

Hi @MElha.1​ 

ST deliver a complete documentation and demo for this use case :

https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_principle

https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

That seems to be very helpful, thank you very much Oliver.

The example is based on the distribution package which I didn't use before, so I am working on it and will give you a feedback if I have any further problems or questions.. thanks again.

M. Elhawy

I have been working on this topic for a while and the "How to exchange large data buffers with coprocessor" example helped me a lot, I modified both the M4 firmware and the linux application to suit my needs but now I am stuck again figuring out the maximum transfer rate that can be achieved (From SRAM to DDR via DMA), it is not clear on the example and principle pages what transfer rates can be achieved, the rate which is referred to in the example is affected by data packing algorithm which seems to consume a lot of time and not the actual transfer rate between memories.

I have reached a rate of 40 MBytes/s when I got rid of the packing algorithm, sampling issues, and saving the data to sd card (Just copying a fixed array of data to the same DDR buffer every time). Is there any way to reach higher speeds as I am looking for speeds that exceed 100 MBytes/s?

Olivier GALLIEN
ST Employee

​Hi @MElha.1​ 

As a example we achieved 65MB/s on the provided "How to exchange large data buffers with coprocessor" exemple by removing compression on M4 side and backup in FS on Linux side.

Maximum b/w achievable is really dependant on use case and implementation. We cannot guarantee to exceed 100MB/s.

In order to identify potential bottleneck in your implementation we need to know better about your use case.

Could you share some details about implementation : DMA managment, RAM and DDR buffer size used etc ?

If you agree, sharing your complete application by private message could also be a very useful option.

BR,

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi Oliver,

Thank you very much for your fast reply. After reading your reply and knowing that 65MB/s is achievable, I optimized the DMA configuration and that made me reach about 60MB/s and I then discovered that the real bottle neck in the example and also in my use case is using the same DMA engine for both transfers from GPIO to SRAM and from SRAM to DDR; With the first stream (GPIO to SRAM) having higher priority it can greatly affect the transfer speed of the second lower priority stream from SRAM to DDR specially when increasing the sampling rate. Even a sampling rate of 15 MSample/s can't be achieved by this configuration and results in failure on the second DMA stream to DDR. One solution I made for this problem is configuring one DMA engine for the transfer from the GPIO to the SRAM and the other DMA engine for the transfer from the SRAM to DDR, with this configuration I reached transfer rates to DDR of higher than 120 MB/s without having problems also with a sampling rate from the GPIOs of 40 MSample/s.

BR,

Elhawy

Hi @MElha.1​ 

Thanks for feedback.

Do you mean you allocate DMA1 to M4 context ?

Thx

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi Oliver,

Yes I allocated both DMA0 and DMA1 to M4 context, one DMA is used to transfer data from the GPIO to SRAM, and the other is used to transfer the data from the SRAM to DDR, now I have a maximum speed of 160 MB/s for the transfer from the SRAM and DDR.

BR,

Elhawy