cancel
Showing results for 
Search instead for 
Did you mean: 

How do I interface mipi dsi 2-lane with 4-lane displays?

KAlab.1
Associate

I cannot find compatible displays for this processor.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
AntonioST
ST Employee

Usually display panels can be configured for the amount of DSI lanes that would be used.

The number of lanes should be specified as one of the properties in the devicetree.

But check carefully while selecting the display. For example, this one only accepts 3 or 4 as value for the property 'dsi-lanes'

https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git/tree/Documentation/devicetree/bindings/display/panel/raydium,rm67191.yaml#n25

Configure the display controller..

Two lanes will limit the total resolution, colour depth and refresh rate.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Two lanes a bit design limiting in a world expecting FHD and UHD displays..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

The datasheet reports:

> LCD-TFT controller, up to 24-bit // RGB888

> – up to WXGA (1366 × 768) @60 fps