cancel
Showing results for 
Search instead for 
Did you mean: 

Getting started with X-LINUX-GNSS1 needs to be updated.

embeddedbro
Associate III

Section 5.1.1 Step 3 says that 

Copy the dts file from the directory: x-linux-gnss1-app\linux-kernel\patch\5.15\kernel to the kernel
source directory at <KERNEL SOURCE PATH>/ arch/arm/boot/dts/

But in the latest X-LINUX-GNSS1 package, the linux kernel is 6.1.11 and there are 3 patch files and 1 fragment file is present. 

It is unclear what to copy exactly. 

@Saurabh.Rawat 

1 REPLY 1
Saurabh.Rawat
ST Employee

Hello @embeddedbro  , 

The Device tree and kernel patches are provided in the 6.1 directory. You can apply them.

Regards,

S