Skip to main content
Associate II
December 2, 2024
Solved

had to use void HAL_GPIO_EXTI_Falling_Callback and void HAL_GPIO_EXTI_Rising_Callback

i used stm32cubeMX to generate code to support GPIO external interrupts.

i expected to use HAL_GPIO_EXTI_Callback and it compiled but did not work.

i had to use HAL_GPIO_EXTI_Falling_Callback and HAL_GPIO_EXTI_Rising_Callback

i used a Nucleo-U5a5ZJ board.

cubeMX  6.12.1

cubeIDE 1.16.1

does anyone know why HAL_GPIO_EXTI_Callback does not work?

I noticed that HAL_GPIO_EXTI_Callback was not in the stm32u5xx_hal_gpio.h file

thanks

phil

 

This topic has been closed for replies.
Karl Yamashita
Karl YamashitaBest answer
Principal
December 3, 2024

There are other STM32's, like STM32G071, STM32C0xx that are the same. 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source

3 replies

Karl Yamashita
Principal
December 3, 2024

ST just made 2 callbacks instead of 1. You can make your own callback and call it. Read the pin status as you would normally

 

uint8_t exti4_pinStatus = 1; // initialize to 1, assuming pin is pulled up

void GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
	if(GPIO_Pin == EXTI_4_Pin)
	{
		exti4_pinStatus = HAL_GPIO_ReadPin(EXTI_4_GPIO_Port, EXTI_4_Pin);
	}
}

void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin)
{
	GPIO_EXTI_Callback(GPIO_Pin);
}

void HAL_GPIO_EXTI_Falling_Callback(uint16_t GPIO_Pin)
{
	GPIO_EXTI_Callback(GPIO_Pin);
}

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Associate II
December 3, 2024

most of your examples say to call

HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)

 

is the STM32_U5xx_hal_gpio.c the only library that does not support this function?

are there any examples that show the use of the code you suggested ?

thanks

phil

 

Karl Yamashita
Karl YamashitaBest answer
Principal
December 3, 2024

There are other STM32's, like STM32G071, STM32C0xx that are the same. 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source