How to create an UART interface in device tree
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-24 10:35 AM
Hello,
I would like to use the UART7 with A7 on the STM32MP157C-DK2 with the openstlinux-20-02-19 ecosystem. Therefore i tried to include/enable the UART interface in the device tree but it is not working correctly.
I configured UART7 in the stm32mp157a-dk1.dts file by setting the status "okay":
&uart7 {
pinctrl-names = "default";
pinctrl-0 = <&uart7_pins_a>;
status = "okay";
};
and in the stm32mp157.c.dtsi file by setting the status "okay":
uart7: serial@40018000 {
compatible = "st,stm32h7-uart";
reg = <0x40018000 0x400>;
clocks = <&rcc UART7_K>;
resets = <&rcc UART7_R>;
status = "okay";
};
An alias was already given:
aliases {
serial0 = &uart4;
serial1 = &usart3;
serial2 = &uart7;
};
I ran bitbake again,flashed the new image to the board and ran the dmesg command.
The following output was generated:
root@stm32mp1-disco:~# dmesg | grep ttySTM*
[ 0.000000] Kernel command line: root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
[ 0.531634] 4000e000.serial: ttySTM3 at MMIO 0x4000e000 (irq = 24, base_baud = 4000000) is a stm32-usart
[ 0.531934] serial serial0: tty port ttySTM3 registered
[ 0.533538] 40010000.serial: ttySTM0 at MMIO 0x40010000 (irq = 25, base_baud = 4000000) is a stm32-usart
[ 1.476144] console [ttySTM0] enabled
[ 5.672859] systemd[1]: Unnecessary job for dev-ttySTM0.device was removed.
It seems that UART7 is not registered nor enabled.
Does Yocto compile a .dtb file or do I have to take additional steps?
I kindly ask you for support. Best wishes
Solved! Go to Solution.
- Labels:
-
STM32MP15 Lines
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-26 8:51 AM
Hello @PSchw.16​
You can check for the dtb build result with the following command on the host PC, in the deploy image directory of the yocto build:
$ dtc -I dtb -O dts stm32mp157c-dk2.dtb
It will give you the dt values in human format.
You can then check for the status of the serial@40018000 node.
Following the result, it will be build issue, or dt apply issue at kernel boot.
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-24 12:01 PM
Do you see any USART related error messages in dmesg?
Yocto should re-build the device tree. Here you find more about that: https://stackoverflow.com/questions/38917745/quick-rebuild-of-device-tree-only-with-yocto-bitbake
You should check the timestamps of relevant files to check if they were rebuild.
Your .dts source looks reasonable. Similar code works on my DK2 (using buildroot).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-25 12:20 AM
Dear @PSchw.16​
Please have a look to the wiki page https://wiki.st.com/stm32mpu/wiki/Trace_and_debug_scenario_-_UART_issue to help for debugging.
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-26 1:40 AM
Hello KnarfB,
thank you for your fast response.
I rebuilt the device tree and the process seemed to work properly now. The timestamps of the files are up to date.
I tried flashing the SDcard with "FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv" via STCubeProgrammer, but it seems to me that something went wrong:
After flashing the SDcard the .dtb-files on the board were not updated although the .dtb-files on the host PC are up to date.
-rw-r--r-- 1 root root 71751 Mar 9 2018 stm32mp157a-dk1.dtb
-rw-r--r-- 1 root root 73626 Mar 9 2018 stm32mp157c-dk2-a7-examples.dtb
-rw-r--r-- 1 root root 74162 Mar 9 2018 stm32mp157c-dk2-m4-examples.dtb
-rw-r--r-- 1 root root 73578 Mar 9 2018 stm32mp157c-dk2.dtb
So the mistake may be the way I flash my device.
I would be very thankful if you could provide the way you flashed/updated your device tree.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-26 8:02 AM
Hello JeanPhilippeR,
thank you for answering my question. I tried to follow the steps given in the article to check the UART probe and I got the following outputs:
root@stm32mp1-disco:~# cat /proc/device-tree/soc/serial\@40018000/status
disabled
root@stm32mp1-disco:~# dmesg | grep 40018000
root@stm32mp1-disco:~# ls -l /proc/device-tree/aliases/*
-r--r--r-- 1 root root 23 Aug 18 01:38 /proc/device-tree/aliases/ethernet0
-r--r--r-- 1 root root 8 Aug 18 01:38 /proc/device-tree/aliases/name
-r--r--r-- 1 root root 21 Aug 18 01:38 /proc/device-tree/aliases/serial0
-r--r--r-- 1 root root 21 Aug 18 01:38 /proc/device-tree/aliases/serial1
-r--r--r-- 1 root root 21 Aug 18 01:31 /proc/device-tree/aliases/serial2
-r--r--r-- 1 root root 21 Aug 18 01:38 /proc/device-tree/aliases/serial3
root@stm32mp1-disco:~# cat /proc/device-tree/aliases/serial2
/soc/serial@40018000
Serial2 is correctly associated with UART7 (@4001800) but the status of @4001800 is "disabled"...am I missing something to enable the UART7?
What surprises me is the fact that there is somehow a serial3 although I haven't defined this alias in the corresponding .dts file.
I hope you might have an idea what is going wrong and I am looking forward to your answer.
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-26 8:51 AM
Hello @PSchw.16​
You can check for the dtb build result with the following command on the host PC, in the deploy image directory of the yocto build:
$ dtc -I dtb -O dts stm32mp157c-dk2.dtb
It will give you the dt values in human format.
You can then check for the status of the serial@40018000 node.
Following the result, it will be build issue, or dt apply issue at kernel boot.
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-26 11:12 AM
Hello @JeanPhilippeR​ ,
after running your recommended command I was able to identify the error as a build issue.
I converted the .dtb file into a text file with "$ dtc -I dtb -O dts -o <filename> and set the status of the UART7 from "disabled" to "okay".
Afterwards I converted my text file back into a .dtb file with "$ dtc -I dtc -O dtb -o <filename>" and replaced the incorrect .dtb files on my board.
Now the serial interface ttySTM2 exists and can be configured.
Thank you so much for your support.
Best wishes