cancel
Showing results for 
Search instead for 
Did you mean: 

WB05KN vs WB05KZ, custom firmware

Dadigno
Senior

Hi everyone,

I'm working with the WB05KN because I’d like to take advantage of the option to have the firmware preloaded during production.
However, I also want to make sure that I’ll be able to load a custom firmware in the future. Is this possible?

I tried flashing the BLE_TransparentMode_SPI and BLE_TransparentMode firmwares from the examples for NUCLEO_WB05KZ, but without success — the firmware gets stuck inside SystemClock_Config.

 

  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

 

 I understand that the two components have different part numbers, but my understanding is that the only difference is the pre-flashed firmware — or is there something else that differentiates them?

 

0 REPLIES 0