2021-07-28 12:34 AM
Example: BLEHeartRateFreeRtos.
In one case of command response we get TL_BLEEVT_CS_OPCODE , another one is TL_BLEEVT_CC_OPCODE.
What is the difference?
Can we get more than one packet of response in each case? (It looks like the code is written to handle this case)
Why in TL_BLEEVT_CC_OPCODE only saves (memcopy) the last packet received ?
while(local_cmd_status == HCI_TL_CmdBusy)
{
hci_cmd_resp_wait(HCI_TL_DEFAULT_TIMEOUT);
/**
* Process Cmd Event
*/
while(LST_is_empty(&HciCmdEventQueue) == FALSE)
{
LST_remove_head (&HciCmdEventQueue, (tListNode **)&pevtpacket);
if(pevtpacket->evtserial.evt.evtcode == TL_BLEEVT_CS_OPCODE)
{
pcommand_status_event = (TL_CsEvt_t*)pevtpacket->evtserial.evt.payload;
if(pcommand_status_event->cmdcode == opcode)
{
*(uint8_t *)(p_cmd->rparam) = pcommand_status_event->status;
}
if(pcommand_status_event->numcmd != 0)
{
local_cmd_status = HCI_TL_CmdAvailable;
}
}
else // my comment: if( TL_BLEEVT_CC_OPCODE)
{
pcommand_complete_event = (TL_CcEvt_t*)pevtpacket->evtserial.evt.payload;
if(pcommand_complete_event->cmdcode == opcode)
{
hci_cmd_complete_return_parameters_length = pevtpacket->evtserial.evt.plen - TL_EVT_HDR_SIZE;
p_cmd->rlen = MIN(hci_cmd_complete_return_parameters_length, p_cmd->rlen);
memcpy(p_cmd->rparam, pcommand_complete_event->payload, p_cmd->rlen);
}
if(pcommand_complete_event->numcmd != 0)
{
local_cmd_status = HCI_TL_CmdAvailable;
}
}
}
}Could not find the relevant documentation.