cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55 Thread

LongHoang
Associate

Dear support team,

 

I was trying to build a thread device with a nucleo-wb55rg board. I did the following steps:

- Implement Full chip erase

- Upgrade firmware STM32Cube_FW_WB_V1.17.3\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_Thread_FTD_fw.bin at address 0x08083000. I referred to the release note, the firmware version is V1.17.1

- Download example Thread_Cli_Cmd and build/upload

- I got it running but it says the radio failed and many issues exist. Please have a look at the attached image.

Please help me check it. What should I do?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @LongHoang and welcome to the ST Community.

I suggest you use the Thread_RCP_Cli_Cmd as recommended on this WIKI. Also, I suggest you use the last version of the firmware STM32Cube_FW_WB_V1.18.0.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.