cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55 CPU2 flash size

metal2oxide
Associate II

How much flash memory is allocated for CPU2 flash and is it possible to write a RF firmware without involvement of CPU2

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

CPU2 is not designed to run user code. It is allocated the second half of the flash by default, although this is adjustable.

If you feel a post has answered your question, please click "Accept as Solution".
BSANT.17
Associate II

Hi,

Allocation depends on RF stack you choose. You can find RF firmware size on %HOMEPATH%\STM32Cube\Repository\STM32Cube_FW_WB_V1.12.1\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\

I think you can't use RF with CPU1 only.

metal2oxide
Associate II

what is the minium allocation which needs to be done for second core. I want CPU1 core to use the max flash