2019-05-07 1:39 AM
Hello everyone,
I have a question in APP_BLE_Init( ). I add
HW_TS_Create(CFG_TIM_PROC_ID_ISR,
&(BleApplicationContext.SwitchOffGPIO_timer_Id),
hw_ts_SingleShot,
Switch_OFF_GPIO); and HW_TS_Start(BleApplicationContext.SwitchOffGPIO_timer_Id, (uint32_t)LED_ON_TIMEOUT); just like the BLE_p2pServer example but
the code didn't run in the Switch_OFF_GPIO() call back function.
Do i need some setting about tImer?
Thank you.
2020-04-10 4:36 PM
Hi, @Htzuh i get exactly the same issue. Did you solve it?
regards