2019-05-16 1:17 AM
I've deleted entire FLASH memory of STM32WB55 during testing. Is there a way to restore FUS and with that the wireless binaries?
As I understand they are encrypted so just writing them isn't working. Is there some tool to do that?
2021-01-25 5:59 AM
@J�?nis Skujenieks
I'm having the same issue here.
My device returns 0x20030030 = 00000000, because i've deleted the memory.
Did you find any solution for the problem?
2021-01-25 6:19 AM
The only solution would be to get FUS in plaintext and flash it yourself, but I don't think this will ever happen. At least officially from ST side.
2021-01-25 6:26 AM
@J�?nis Skujenieks
So, does that mean I lost my development board? I can't get it back.
2021-01-25 6:43 AM
If you truly erased whole flash (cleared ESE bit), then as far as I know there is no way to restore FUS and wireless binaries.
2021-01-25 6:52 AM
@J�?nis Skujenieks Ok! Thanks for the help!
2021-01-25 12:59 PM
For us we followed the user guide or readme that explained how to load the M0 software using the STM32_Programmer_CLI.exe utility. The guide outlined numerous steps and for us this worked (I think steps 1-2 were like setting up the input conditions to go into this loading mode):
cd "C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin"
### Step 3
STM32_Programmer_CLI.exe -c port=usb1 -fwdelete
### Step 4
STM32_Programmer_CLI.exe -c port=usb1 -r32 0x20030030 1
### Step 5
STM32_Programmer_CLI.exe -c port=usb1 -fwupgrade "<YOUR_PATH>\STM32Cube_FW_WB_V1.2.0\Projects\STM32WB_Copro_Wireless_Binaries\stm32wb5x_FUS_fw.bin" 0x080EC000 firstinstall=0
### Step 6
STM32_Programmer_CLI.exe -c port=usb1 -fwupgrade "<YOUR_PATH>\STM32Cube_FW_WB_V1.2.0\Projects\STM32WB_Copro_Wireless_Binaries\stm32wb5x_BLE_Stack_fw.bin" 0x080CC000 firstinstall=1
Note that you may prefer a newer firmware version than what I had here. Also, I dont know if this solves things if you managed to completely erase the flash. I think I tried it once but was unsuccessful and then this procedure worked for us.
2021-01-26 3:55 AM
@ [Michael Bauer]@Michael Bauer
When I execute the commands I received these responses:
For STEP 3:
Error: FUS_STATE_ERR_UNKNOWN
Firmware delete n░1 failed after retrying!
Error: fwdelete Operation Failure! Please, try again
For STEP 4:
Reading 32-bit memory content
Size : 4 Bytes
Address: : 0x20030030
0x20030030 : 00000000
Indicates that the FUS has been deleted.
How to program FUS if the returns of STEP 4 is 00000000?