2020-12-08 4:16 PM - last edited on 2026-01-21 12:50 PM by Andrew Neil
Hello
i made a customised board using the STM32L476RETx mcu with a lora module : DORJI DRF1262T
I opened the project from i-cube-lrwan expansion package with the name SX1262dvk1das USING THE SX1262 AT 868MHz.
i updated the PINOUT of my MCU and exclude all unnecessary driver and board sensor not used.
when i compile, everything is OK with error and warnings
i program my board. the program run but in 4s112ms the program is bloqued and the message in the UART of " 4s112 ms PHY txTimeOut " is printed and everything is stopped.
SPI pin and CS and DIO1 are well connected and in the beginningof the run, i see a signal on this protocole. the board well worked in ping pong mode with another board
Please help
Thank you
2020-12-08 4:43 PM
https://community.st.com/s/question/0D53W00000JNMqBSAX/lora-sx1262-tx-timeout