cancel
Showing results for 
Search instead for 
Did you mean: 

How to intergate functionnalities to the stack Lora (end node)

SBour.9
Associate II

Hi,

I wrote a code using an uart with a circular Rx dma and idle interupt to communicate with a sensor. The config is working fine alone and now i want to include it into the project End Node form the LoRa package. But i cannot figure out why it's not working.

I am able to send characters with the UART but i can't recieve anything from the DMA.

If i disable my dma and use the uart in polling mode for reception it is working fine but when i add the dma nothing append.

I am working with the STM32L073RZ and expension board SX1272MB2DAS.

The uart i want to use is the USART4 with rs485 flow control (Tx => PC10, Rx=>PC11, DE=>PA15) . I checked, there is no GPIO conflict with the expension board.

Any ideas for a solution? I feel like there could be some conflicts with the DMA since it's use for vcom. Or maybe there is an other file in the loRa stack i need to modify ?

Simon

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0