cancel
Showing results for 
Search instead for 
Did you mean: 

Discrepancy in AN5481 Lorawan AT Commands for ST32cube

DavidG7
Associate II

The parameters  for the AT+TCONF are shown differently in your example to where you show the breakdown of the individual paramters.

In your example you show the <cr. parameter on the command line as 4/5  

868000000:14:125:12:4/5:0:0:1:255:0:0:0

where in the description of the parameters on page 28 you show that 1:  represents 4/5, so shouldn't command line look like this instead   

868000000:14:125:12:1:0:0:1:255:0:0:0

 

 

 

0 REPLIES 0