2020-04-03 12:44 AM
Hi Guys,
I have problems reading. I have followed the STM32WB Workshop on stm32wb (using mx version 5.4.0). Now i'm trying to read but all examples seem to only use notifying and writing.
I have the following char created and added some default value.
aci_gatt_add_char(SvcHandle,
UUID_TYPE_128, &uuid16,
1,
CHAR_PROP_READ | CHAR_PROP_WRITE_WITHOUT_RESP,
ATTR_PERMISSION_NONE,
GATT_NOTIFY_ATTRIBUTE_WRITE | GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP,
10,
0,
&(AlarmThresholdHandle));
uint8_t pData[1] = {59};
aci_gatt_update_char_value(SvcHandle,
AlarmThresholdHandle + 1,
0, /* charValOffset */
1, /* charValueLen */
pData);
Within server app handler it enters this case when im reading, and found the right handler. This is the part where i get lost, what to do next? I implemented the following but that does not work.
case EVT_BLUE_GATT_READ_PERMIT_REQ:
{
aci_gatt_read_permit_req_event_rp0* attributeToRead;
attributeToRead = (aci_gatt_read_permit_req_event_rp0*)blue_evt->data;
if(attributeToRead->Attribute_Handle == AlarmThresholdHandle + 1)
{
uint8_t pData[1] = {5};
retval = aci_gatt_update_char_value(SvcHandle,
AlarmThresholdHandle + 1,
0, /* charValOffset */
1, /* charValueLen */
pData);
}
returnValue = SVCCTL_EvtAckFlowEnable;
}Once i passed here i cant trigger any new events anymore.
I would like to see some examples of reading or get some feedback on which steps to preform to read successfully.
Thanks in advance,
Solved! Go to Solution.
2020-04-09 12:59 AM
Read request must always be completed with
(void)aci_gatt_allow_read(read_permit_req->Connection_Handle);
switch(event_pckt->evt)
{
case EVT_VENDOR:
{
blue_evt = (evt_blue_aci*)event_pckt->data;
switch(blue_evt->ecode)
{
case EVT_BLUE_GATT_READ_PERMIT_REQ:
{
read_permit_req = (aci_gatt_read_permit_req_event_rp0*)blue_evt->data;
if(read_permit_req->Attribute_Handle == (aTemplateContext.TemplateReadClientToServerCharHdle + 1))
{
memset(MsgResponse, 0x22, 87);
ReadCount++;
HAL_GPIO_TogglePin(LED1_GPIO_PORT, LED1_PIN);
(void)aci_gatt_allow_read(read_permit_req->Connection_Handle);
#if 1
aci_gatt_update_char_value(aTemplateContext.TemplateSvcHdle,
aTemplateContext.TemplateReadClientToServerCharHdle,
0, /* charValOffset */
87, /* charValueLen */
(uint8_t *) MsgResponse);
return_value = SVCCTL_EvtNotAck;
#endif
}
break;
}for example: See the code snipped below that I worked and found useful:
2020-04-09 12:47 AM
You may have a look at the blood presure project here:
STM32Cube_FW_WB_V1.5.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_Peripheral_Lite
The related characteristic has a READ property.
2020-04-09 12:59 AM
Read request must always be completed with
(void)aci_gatt_allow_read(read_permit_req->Connection_Handle);
switch(event_pckt->evt)
{
case EVT_VENDOR:
{
blue_evt = (evt_blue_aci*)event_pckt->data;
switch(blue_evt->ecode)
{
case EVT_BLUE_GATT_READ_PERMIT_REQ:
{
read_permit_req = (aci_gatt_read_permit_req_event_rp0*)blue_evt->data;
if(read_permit_req->Attribute_Handle == (aTemplateContext.TemplateReadClientToServerCharHdle + 1))
{
memset(MsgResponse, 0x22, 87);
ReadCount++;
HAL_GPIO_TogglePin(LED1_GPIO_PORT, LED1_PIN);
(void)aci_gatt_allow_read(read_permit_req->Connection_Handle);
#if 1
aci_gatt_update_char_value(aTemplateContext.TemplateSvcHdle,
aTemplateContext.TemplateReadClientToServerCharHdle,
0, /* charValOffset */
87, /* charValueLen */
(uint8_t *) MsgResponse);
return_value = SVCCTL_EvtNotAck;
#endif
}
break;
}for example: See the code snipped below that I worked and found useful:
2020-04-09 7:01 AM
Exactly where i was looking for, thanks!
2020-11-26 1:16 PM
Thanks, thats it...... and my Problem is past now ....
2023-03-01 12:25 AM
Hello,
I just read your post on how to send message usi g BLE in STM32. Can you please help me know where I can include my alue so that I may be able to send using BLE. Thank you in advance.
Regards,
M.K