cancel
Showing results for 
Search instead for 
Did you mean: 

B-L072Z-LRWAN1

Snm.1
Associate III

I am using B-L072Z-LRWAN1. I ran the ping pong application ready here. I wanted to set up timer interrupt myself but there is no .ioc file. I opened another project, set up a timer in cubemx, tried and run it, and added it to the ping pong project. but timer interrupt ping pong did not work in the project. I wonder if you have a solution.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

The code was written by an engineer, not code-generated, and based on Semtech's model, not ST's

Add the TIM code as if you were using the HAL directly.

Look at the HAL TIM examples

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Snm.1
Associate III

hello I just added the state code but I couldn't run it. I wonder if I'm trying to use a timer that I shouldn't use. I used timer 2-3-4. I am working for my university project. I will be glad if you help.

Snm.1
Associate III

hello I just added the state code but I couldn't run it. I wonder if I'm trying to use a timer that I shouldn't use. I used timer 2-3-4. I am working for my university project. I will be glad if you help.