cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747-DISCO with TouchGFX 4.14.0

EnricoP
Associate III

Good morning,

I'm using a discovery board STM32H747-DISCO.

Why, Touchgfx don't generate the project .ioc, to import in CUBE IDE?

Instead, if I select another board (for example STM32F7508-DK) , when generate code, the compiler buil also .ioc file.

I have also installed the last version 4.14.0 of TouchGFX, but the problem persist.

Thank you

This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
Romain DIELEMAN
ST Employee

Hi,

TouchGFX 4.17 is now live along a new release of the TouchGFX Board Setup (new name for "Application template") for the STM32H747-disco board based on STM32CubeMX and with a STM32CubeIDE project.

/Romain