cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 5.5.0/ TouchGFX 4.13.0 Framebuffer Allocation

KSait.1
Associate

I have switched from TouchGFX 4.12 to the latest 4.13.0.

At the TouchGFXGeneratedHAL.cpp, I found a following line in the

void TouchGFXGeneratedHAL::initialize() function.

uint32_t frameBuf[(800 * 480 * 2 + 3) / 4] LOCATION_ATTRIBUTE("TouchGFX_Framebuffer"); 

(The actual number of allocation is depends on LCD width, height, and bit depth)

This is not in the old version, for example at the file, STM32H7HAL.cpp

Since the allocation uses too much RAM, I am facing linker error.

Are there any ways to fix the problem?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
KSait.1
Associate

I found former project uses SDRAM. This question is based on many misunderstandings. Sorry for bothering this forum.