2022-07-14 2:10 AM
I hope this is the right section of the site to ask this question, otherwise please redirect this thread.
I just started programming, I am using a 20x04 LCD with stm32F407G and I need the classic function "
lcd_i2c_setCursor (row, col); ". I am not able to implement it by modifying the one already in the 16x02 display library.
So I am asking if you can redirect/send me to a post or link where this function is explained for 20x04 or if someone already has it and can attach the code so that I can "copy-paste" it into my project.
Or if there is a way to modify the function " lcd_i2c_setCursor (row, col); " that I have for the 16x02 LCD ... we can modify it here together:
void lcd16x2_i2c_setCursor(uint8_t row, uint8_t col)
{
uint8_t maskData;
maskData = (col)&0x0F;
if(row==0)
{
maskData |= (0x80);
lcd16x2_i2c_sendCommand(maskData);
}
else
{
maskData |= (0xc0);
lcd16x2_i2c_sendCommand(maskData);
}
}Thank you.
2022-12-26 5:14 AM
Hello @luke514 ,
You can refer to this example.
Please find the attachment the I2C-lcd libraries.
/* USER CODE BEGIN 2 */
lcd_init();
lcd_send_cmd (0x80|0x00);
lcd_send_string("FIRST");
lcd_send_cmd (0x80|0x40);
lcd_send_string("SECOND");
lcd_send_cmd (0x80|0x1C);
lcd_send_string("THIRD");
lcd_send_cmd (0x80|0x54);
lcd_send_string("FINISH");
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
for (int i=0; i<5; i++)
{
lcd_send_cmd (0x1C); // display shift right
HAL_Delay(350);
}
for (int i=0; i<5; i++)
{
lcd_send_cmd (0x18); // display shift left
HAL_Delay(350);
}
}
/* USER CODE END 3 */Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-08 1:04 PM
Thank you for your reply! I finally managed a few weeks ago to find the function I needed.