cancel
Showing results for 
Search instead for 
Did you mean: 

Is TouchGFX only for STM32, it's possible to run an TouchGFX app on Linux, Raspberry?

PCarv.2
Associate

This is probably the stupidest question asked here but, i want to be absolutely sure.

It's TouchGFX only for smt32 microcontroller? or can i use TouchGFX with a Esp32 for instance?. 

And, there is a way to develop a desktop aplication with tochGFX, can i develop an app for running on a Raspberry Pi?. tanks so much.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @PCarv.2​, to the community!

TouchGFX is only available for STM32 and currently only runs under Windows. 

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @PCarv.2​, to the community!

TouchGFX is only available for STM32 and currently only runs under Windows. 

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Peter BENSCH
ST Employee

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.