2024-06-24 07:29 AM
Hi TouchGfx Team,
Could you please consider adding a menu item to start MSVS project \simulator\msvs\Application.sln ? Ideally a keyboard shortcut as well.
Thank you
Ferro
2024-06-25 02:46 AM
Hello @ferro ,
What exactly do you want?
A way to start the simulator debugger in Studio code from the Designer (just like we have "Run simulator", you want something like "Run simulator debugger in Studio code")?
And maybe a way to start it from Designer with a keyboard shortcut?
Regards,
2024-06-25 02:58 AM
>""Run simulator debugger in Studio code""
What I mean is the same functionality as when I double click on Application.sln file i.e. MSVC IDE opens.
I do not want to run MSVC Simulator ie executing the code, just to open the .sln project so that I do not need to navigate to it in File manager.
Thank you
2024-06-25 03:01 AM - edited 2024-06-25 03:04 AM
Sth like this, I click 'Open files in MS Visual Studio' (and if still available some Fx key or a combo Ctrl+XY)
And MSVC IDE opens
2024-06-25 03:03 AM
Ok, so the ability to open the Visual Studio project from within Designer, either from a button or from a keyboard shortcut.
I will inform the team and keep you updated.
Regards,
2024-06-25 03:18 AM
That is correct, thank you.