Skip to main content
rutvij
Associate
October 6, 2016
Question

Getting hardfault using stemwin GUIDRV_FlexColor driver for st7735 in stm32f407vg EVM after LCD_X_DisplayDriver()

  • October 6, 2016
  • 1 reply
  • 2033 views
Posted on October 06, 2016 at 09:38

Hello Folks,

I am working on stm32f407vg EVM, I have interfaced MIDAS LCD using SPI. The LCD has ST7735s controller.

Now I am able to make manual patterns of check box, circle and screen colour randomly but I need GUI to be implemented so I have chosen STemWin library , the library is ''STemWin522_CM4_IAR''. I read the user & reference guide of stemwin and found that I can go with ''GUIDRV_FlexColor'' drivers.

I have done configurations in LCDconf.c (I have attached here). In GUIconf.c  my configurations are as per below.

&sharpdefine GUI_NUMBYTES  (1024) *  15

//

// Define the average block size

//

&sharpdefine GUI_BLOCKSIZE   0x128

I have initialised LCD controller before GUI_INIT(), I have also added ''RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_CRC, ENABLE);''

But unfortunately after returning from ''LCD_X_DisplayDriver()'' function I am getting Hard fault so I need to understand why I am getting hard-fault and is there any issue in my configurations ?

Please let me know if I can provide you more details.

Any Help on this issue would be great appreciable.

Thanks & Regards,

Rutvij

----------------------------------------------------------------------

File        : LCDConf.c

Purpose     : Display driver configuration file

----------------------------------------------------------------------

*/

/**

  &sharpinclude <string.h>

/* GUI main init as per StemWin */

&sharpinclude ''GUI.h''

/* As per STemWin 5 doc ST7735 Contoler IC's driver config */

&sharpinclude ''GUIDRV_FlexColor.h''

/* For callback registers of LCD */

&sharpinclude ''MCT0144C6W128128PML_App.h''

/*********************************************************************

*

*       LCD_X_Config

*w

* Purpose:

*   Called during the initialization process in order to set up the

*   display driver configuration.               

*   

*/

static void LcdWriteReg(U16 Data) {

  // ... TBD by user

    SPI_sendCommand(Data);

}

static void LcdWriteData(U16 Data) {

  // ... TBD by user

    SPI_sendData(Data);

}

static void LcdWriteDataMultiple(U16 * pData, int NumItems) {

  while (NumItems--) {

    // ... TBD by user

      SPI_sendData((uint8_t)*pData++);

  }

}

static void LcdReadDataMultiple(U16 * pData, int NumItems) {

  while (NumItems--) {

    // ... TBD by user

      *pData++=SPI_sendData(0x00);

  }

}

void LCD_X_Config(void)

{

   GUI_DEVICE *pDevice = NULL;

   CONFIG_FLEXCOLOR Config = {0};

   GUI_PORT_API PortAPI = {0};

  /* Set display driver and color conversion */

  /* 16 BPP configuration for st7735s */

  /*  from specificaly LCD side configure LCD to work on the same BPP

      This can be done by cofiguring LCD internal register go into

      ''ST7735_COLMOD'' in ''MCT0144C6W128128PML_App.c'' file

   */

  /* for RGB - GUICC_M565 ,  for BGR - GUICC_565*/

  pDevice = GUI_DEVICE_CreateAndLink(GUIDRV_FLEXCOLOR, GUICC_M565, 0, 0);

   

  //

  LCD_SetSizeEx (0, LCD_WIDTH , LCD_HEIGHT);

  LCD_SetVSizeEx(0, LCD_WIDTH, LCD_HEIGHT);

 

  //

  // Orientation

  //

  Config.Orientation = GUI_SWAP_XY | GUI_MIRROR_Y;

  GUIDRV_FlexColor_Config(pDevice, &Config);

  // Set controller and operation mode

  //

 

  PortAPI.pfWrite16_A0  = LcdWriteReg;

  PortAPI.pfWrite16_A1  = LcdWriteData;

  PortAPI.pfWriteM16_A1 = LcdWriteDataMultiple;

  PortAPI.pfReadM16_A1  = LcdReadDataMultiple;

  /* GUIDRV_FLEXCOLOR_F66709 - for st7735 */

  /* GUIDRV_FLEXCOLOR_M16C0B8 16bpp, no cache, 8 bit bus - SPI data bus */

  GUIDRV_FlexColor_SetFunc(pDevice, &PortAPI, GUIDRV_FLEXCOLOR_F66709, GUIDRV_FLEXCOLOR_M16C0B8);

      

}

/*********************************************************************

*

*       LCD_X_DisplayDriver

*

* Purpose:

*   This function is called by the display driver for several purposes.

*   To support the according task the routine needs to be adapted to

*   the display controller. Please note that the commands marked with

*   'optional' are not cogently required and should only be adapted if

*   the display controller supports these features.

*

* Parameter:

*   LayerIndex - Index of layer to be configured

*   Cmd        - Please refer to the details in the switch statement below

*   pData      - Pointer to a LCD_X_DATA structure

*

* Return Value:

*   < -1 - Error

*     -1 - Command not handled

*      0 - Ok

*/

int LCD_X_DisplayDriver(unsigned LayerIndex, unsigned Cmd, void * pData)

{

     int r;

  (void) LayerIndex;

  (void) pData;

 

 

  switch (Cmd)

  {

 

    /*

     * Called during the initialization process in order to set up the

     * display controller and put it into operation.

     */  

    case LCD_X_INITCONTROLLER:

    {

      return 0;

    }

    default:

        {

            r = -1;

            

        }

          

  }

  return r;

}

/*************************** End of file ****************************/

#stemwin #stm32f407vg #st7735
This topic has been closed for replies.

1 reply

slimen
Visitor II
October 6, 2016
Posted on October 06, 2016 at 19:02

Hello,

Refer to this [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Problem%20getting%20STemWin%20to%20work%20with%20RA8875-Based%20LCD&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=338]thread and

http://forum.segger.com/index.php?page=Thread&threadID=2435

, may help you on this issue.

Regards