cancel
Showing results for 
Search instead for 
Did you mean: 

Demo source code of touchgfx_demo2014_240x320

Stormblessed
Associate

I'm looking for the source code of touchgfx_demo2014_240x320, I could only find the .hex file for the STM32F429I-Discovery board. It used to be available in old versions of TouchGFX designer under <touchgfx install dir>/app/demo/. Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Martin KJELDSEN
Chief III

Hi @Stormblessed​,

Here's the code. The application structure is based on 4.8.0, though, so it does not follow the usual structure where touchgfx framework is inside the application folder. You may be able to upgrade it, or at the very least, get the source code from the gui/ folder.

/Martin

View solution in original post

3 REPLIES 3
Martin KJELDSEN
Chief III

Hi @Stormblessed​,

Here's the code. The application structure is based on 4.8.0, though, so it does not follow the usual structure where touchgfx framework is inside the application folder. You may be able to upgrade it, or at the very least, get the source code from the gui/ folder.

/Martin

Stormblessed
Associate

Thanks for your fast reply, that's what I needed.

S

Martin KJELDSEN
Chief III

No problem! Let me know if you need anything else and if you can get the demo working with Touchgfx 4.10.0

/Martin