2018-02-20 8:36 AM
I want graphic primitives like text on layer 2 to be superimposed on top of the image in layer 1. I want to do this will full alpha values of 255 for both layers.
I wrote the text against a color I made transparent using the colorkeying function which works great. But layer 1 is still never exposed unless I blend the images. I thought using black as a default layer color made it transparent to layers below? So I thought all alpha=0 graphic elements on layer 2 would allow layer 1 to show fully, while alpha=255 graphic element on layer 2 would completely obscure layer 1?
Can this be done? Does it require the use of the the Chrome-Art Accelerator? I've attached my config code.
Thanks!
hltdc.Instance = LTDC;
hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL; hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL; hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL; hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC; hltdc.Init.HorizontalSync = 47; hltdc.Init.VerticalSync = 2; hltdc.Init.AccumulatedHBP = 135; hltdc.Init.AccumulatedVBP = 34; hltdc.Init.AccumulatedActiveW = 935; hltdc.Init.AccumulatedActiveH = 514; hltdc.Init.TotalWidth = 975; hltdc.Init.TotalHeigh = 527; hltdc.Init.Backcolor.Blue = 0; hltdc.Init.Backcolor.Green = 0; hltdc.Init.Backcolor.Red = 0; if (HAL_LTDC_Init(&hltdc) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }pLayerCfg.WindowX0 = 0;
pLayerCfg.WindowX1 = 771; pLayerCfg.WindowY0 = 0; pLayerCfg.WindowY1 = 467; pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_L8; pLayerCfg.Alpha = 255; pLayerCfg.Alpha0 = 0; pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA; pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA; pLayerCfg.FBStartAdress = (uint32_t)&pic1; pLayerCfg.ImageWidth = 771; pLayerCfg.ImageHeight = 467; pLayerCfg.Backcolor.Blue = 0; pLayerCfg.Backcolor.Green = 0; pLayerCfg.Backcolor.Red = 0; if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }pLayerCfg1.WindowX0 = 0;
pLayerCfg1.WindowX1 = 670; pLayerCfg1.WindowY0 = 0; pLayerCfg1.WindowY1 = 445; pLayerCfg1.PixelFormat = LTDC_PIXEL_FORMAT_L8; pLayerCfg1.Alpha = 128; pLayerCfg1.Alpha0 = 0; pLayerCfg1.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA; pLayerCfg1.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA; pLayerCfg1.FBStartAdress = (uint32_t)&field; pLayerCfg1.ImageWidth = 670; pLayerCfg1.ImageHeight = 445; pLayerCfg1.Backcolor.Blue = 0; pLayerCfg1.Backcolor.Green = 0; pLayerCfg1.Backcolor.Red = 0; if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg1, 1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }HAL_LTDC_ConfigColorKeying(&hltdc,0,1);
HAL_LTDC_EnableColorKeying(&hltdc,1);&sharpLT#lcd #ltdc #graphics2018-02-20 9:10 AM
SOLVED
Set BlendingFactor2 = 255 (alpha * pixel) = 255