cancel
Showing results for 
Search instead for 
Did you mean: 

我的开�?��?�是STM32F429I-DISC1 我用TouchGFX 4.20.0 里的STM32F429I模�?��?显示图画为什么?

杨英.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
ChahinezC
Lead

Hello @�?� 英​,

Welcome to STM32 Community.

Thanks to develop your posts in English, it helps us, and the users of our community understand your question and try to help you.

Thanks.

Chahinez.

ChahinezC
Lead

To help in this case, I put your question in google translate:

"My development board is STM32F429I-DISC1, I use the STM32F429I template in TouchGFX 4.20.0 does not show pictures, why?"

I suggest you to check the STM32F429I-DISCO & TouchGFX Setup, to verify the jumpers on the boards and the pins used.

Thank you.

Regards,

Chahinez.

Romain DIELEMAN
ST Employee

Hi,

Could you also check if you are using the correct project in TouchGFX Designer ? As you can see there are 3 different projects for the STM32F429 based on the revision of your board as there were some hardware changes between versions. For example if your board is blue, use the project for the "revision E-01". You should be able to check the revision on a white sticker on your board.

/Romain