cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-CRYPTOLIB cmox_eddsa_verify memory fail

AKole.3
Associate

Hi everyone!

In our project for stm32f446, we are trying to use X-CUBE-CRYPTOLIB to verify the firmware signature on the device using ED25519. Unfortunately, when trying to call the cmox_eddsa_verify method, we get the CMOX_ECC_ERR_MEMORY_FAIL error. The error occurs when memory is allocated. Tell me how to overcome this, or perhaps we are doing something wrong.

Below is the code

bool FirmwareCrypt::verify(const uint8_t* data, size_t size, const uint8_t* sign, size_t sign_size)
{
    if (!data || !size) 
        return false;
    
    cmox_ecc_handle_t handle;
    uint8_t ecc_buf[ECC_BUF_SIZE// 2048];
    uint32_t fault_check = 0;
    memset((void*)&handle, 0, sizeof(cmox_ecc_handle_t));
    cmox_ecc_construct(&handle, CMOX_ECC256_MATH_FUNCS, ecc_buf, ECC_BUF_SIZE);
    
    cmox_ecc_retval_t ret = cmox_eddsa_verify(&handle, CMOX_ECC_CURVE_ED25519, 
        public_key, PUBLIC_KEY_SIZE, data, size/*~100Kb*/, sign, sign_size, NULL/*&fault_check*/);
    
    if (/*(static_cast<uint32_t>(ret) != fault_check) && */(ret != CMOX_ECC_SUCCESS)) {
        return false;
    }
    
    return true;
}

7 REPLIES 7
Jocelyn RICARD
ST Employee

Hello @AKole.3​ ,

in the example provided here STM32CubeExpansion_Crypto_V4.0.1\Projects\NUCLEO-G474RE\Applications\ECC\EDDSA_SignVerify\ I can see:

uint8_t Working_Buffer[2200];

So, maybe setting your buffer size with same value will solve your issue

Best regards

Jocelyn

G'day,

Is there any documentation on how to set this buffer to be the appropriate size? This answer leads me to more questions:

  • Is 2200 always safe?
  • If you set it for one curve / memory implementation will it always work if it works once? 
  • I presume it depends on the ECC curve and the lowmem vs highmem option?

Cheers,

Hamish.

 

Hello @HMcKi ,

if you look at the wiki here you will see the usage of the buffer depending on option used.

So, 2200 looks like a really safe value.

Best regards

Jocelyn

 

Thank you.

Hi Jocelyn, 

Is there any limitation between the length of message and working_buffer, if I provide a message exceeded 4096 bytes, cmox_eddsa_verify always returns CMOX_ECC_ERR_MEMORY_FAIL. In our project, we need to verify the frimware with a length nearly of 256KB.

Do we need to split the firmware to small chunks (like 1023 bytes), and sign them separately, then transfer the chunks and signatues to cmox_eddsa_verify one by one?

BR.

xlongfeng

Hello @xlongfeng ,

The verification of a signature is always done on the hash of the data you want to check.

So, first compute the digest of your firmware using a hash algorithm such as SHA-256.

Then use this digest as input to your verification algorithm

Best regards

Jocelyn

Ajay_Bhatt
Associate

@AKole.3 
Please can you let me know public_key is provided in which format in your code?

Please can you let me know as to how you have generated public key, is it through STM32_KeyGen_CLI.exe?