cancel
Showing results for 
Search instead for 
Did you mean: 

"regression.sh" in "STM32Cube_FW_L5_V1.4.0" can't execute successfully

zqizh.1
Associate III

Hi,

I don't do any change to the script file, please advise how to let the script work normally.

Rgds,

QiZhang

D:\>cd D:\WSL_DIR\STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM\TFM_SBSFU_Boot\STM32CubeIDE

D:\WSL_DIR\STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM\TFM_SBSFU_Boot\STM32CubeIDE>bash regression.sh

regression script started

Regression to RDP 0, enable tz

regression.sh: line 16: $'STM32_Programmer_CLI\r': command not found

regression.sh: line 59: syntax error: unexpected end of file

D:\WSL_DIR\STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM\TFM_SBSFU_Boot\STM32CubeIDE>

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

> my PC OS is win 10 , with WSL2 installed

So, when you type 'bash' it actually runs in the WSL. It does not run on the Windows side. Do you fully understand the consequences?

Maybe you would rather prefer a Windows-native bash such as one that comes with git or Cygwin?

View solution in original post

4 REPLIES 4
Imen.D
ST Employee

Hello @zqizh.1​ ,

I have checked from my side and I cannot reproduce this issue.

Were you able to resolve this ? If yes, it will be interesting to share with us your update.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
zqizh.1
Associate III

Hi,

I have solved it with below work around solution:

1) change "STM32_Programmer_CLI" to"STM32_Programmer_CLI.exe" in line 4

2) remove "\r"

sed 's/\r$//' regression.sh > tmp.sh

mv tmp.sh regression.sh

my PC OS is win 10 , with WSL2 installed.

Please give a formal way.

Rgds,

QiZhang

> my PC OS is win 10 , with WSL2 installed

So, when you type 'bash' it actually runs in the WSL. It does not run on the Windows side. Do you fully understand the consequences?

Maybe you would rather prefer a Windows-native bash such as one that comes with git or Cygwin?

I've followed your instruction, uninstall the WSL2, and install the Cygwin.

$ cd /cygdrive/d/WSL_DIR/STM32Cube_FW_L5_V1.4.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/STM32CubeIDE/

1) run "./regression.sh" no problem.

2) run "./TFM_UPDATE.sh" fail.

Please advise.

Thanks.