cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-IDW01M1 -WHY level shifter is used in the board

chaitanya jasti
Associate II
Posted on February 28, 2017 at 16:50

Hi,

In x-NUCLEO-IDW01M1 -WHY level shifter(3.3v to 2.5v ) is used in the board?

RTS and CTS are tolerent to 5v but it is shifted to 2.5v,why?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on February 28, 2017 at 19:35

Being tolerant and having undesirable current flows are two different things. The boards targets low power / low voltage applications. A significant number of pins aren't tolerant, and a robust design will likely need you to work in the 2.5V domain.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..