cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-SBSFU for L4+

Silvio Barani
Associate II
Posted on June 04, 2018 at 22:36

Hi.

I tried to port latest SBSFU to STM32L4+ line of MCUs using NUCLEO-L4R5ZI board.

I modified preprocessor macro to STM32L4R5xx and I found such problems:

1. FLASH_PAGE_SIZE for L4+ is 0x1000, while for L4 it is 0x0800.

It produces following error:

= [SBOOT] System Security Check successfully passed. Starting...

= [FWIMG] Slot #0 @: 8080800 / Slot #1 @: 800e000 / Swap @: 80f2800

= [FWIMG] slot 0 (8080800) is not properly aligned: please tune your settings

= [FWIMG] swap region (80f2800) is not properly aligned: please tune your settings

========= End of Execution ==========

Fix is simple: aligning memory addresses of SLOT_0 and SWAP to 0x1000.

When all protections are disabled (with SECBOOT_DISABLE_SECURITY_IPS defined) everything works fine.

Unfortunately when I tried to apply some protections I observed next two problems:

2. Inclusion of all protections resulted in linking problem: region `SB_ROM_region' overflowed by 728 bytes.

3. With some protections disabled (SFU_MPU_PROTECT_ENABLE and SFU_TAMPER_PROTECT_ENABLE) it is possible to link SBSFU but rolling reset was observed.

By experimenting I realized that enabling SFU_PCROP_PROTECT_ENABLE or SFU_FWALL_PROTECT_ENABLE causes rolling SBSFU reset.

I'm still investigating those problems, but I'm interested if someone already ported SBSFU to L4+.

Regards

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Sorry, bumping old zombie unanswered questions off my feed

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..