cancel
Showing results for 
Search instead for 
Did you mean: 

writing to a port which is not available

Posted on February 04, 2015 at 07:47

Hello,

we have a small software (bootloader) running on a STM32F103. In a new project, we selecte a ''smaller'' type the STM32F105 with less pins.

In the bootloader we set a push pull port high. On the new controller this port is not existing.

Will it cause any problems writing to a port which is not available on the new STM32F105 type?

It would be a big advantage to use exactly the same code on both devices.

Regards

Leo
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on February 04, 2015 at 14:10

No

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..