cancel
Showing results for 
Search instead for 
Did you mean: 

Why my Nucleo Board doesn't start the program when energized until I press the reset button?

AColl.252
Associate

I'm using STM Cube MX and Keil IDE in order to program my NUCLEO-F334R8 board, the problem is that I have to press the rest button every time I connect the USB port in order to start the main program, What am I configuring wrong? What can I do to fix it?

Greetings.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Should we all just guess? Try not reconfiguring the clocks, and see if it continues to run properly, do some debugging.

Try just building some of the examples under the CubeF3 HAL trees

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Super User

What does "doesn't start" mean? How do you know it isn't "starting"? Is the board powered only from USB?

If you feel a post has answered your question, please click "Accept as Solution".