Skip to main content
arnold_w
Senior II
February 1, 2016
Question

Why is my timer 4 interrupt issued as soon as I enable the interrupt?

  • February 1, 2016
  • 3 replies
  • 635 views
Posted on February 01, 2016 at 10:26

I want to generate an interrupt after 2 seconds and I am running at 32 MHz. However, my interrupt is issued as soon as I enable the interrupt. What am I doing wrong?

void testTimer4(EventCallback_t timerInterruptCallback)
{
timerInterruptCallback_ = timerInterruptCallback;
RCC->APB1ENR |= RCC_APB1ENR_TIM4EN;
TIM4->PSC = 976;
TIM4->ARR = 65505;
TIM4->CNT = 0;
TIM4->SR &= (~TIM_SR_UIF);
TIM4->DIER |= TIM_DIER_UIE;
HAL_NVIC_EnableIRQ(TIM4_IRQn);
TIM4->CR1 |= TIM_CR1_CEN;
}
void TIM4_IRQHandler(void)
{
TIM4->SR &= (~TIM_SR_UIF);
HAL_NVIC_DisableIRQ(TIM4_IRQn);
TIM4->DIER &= (~TIM_DIER_UIE);
TIM4->CR1 &= (~TIM_CR1_CEN);
RCC->APB1ENR &= (~RCC_APB1ENR_TIM4EN);
(void)timerInterruptCallback_((uint32_t)TIMER_4_EXPIRED, 0);
}

    This topic has been closed for replies.

    3 replies

    Radosław
    Associate II
    February 1, 2016
    Posted on February 01, 2016 at 10:36

    You change prescaler, in configuration stage generate software uptade then clear all flags.

    Your code looks very strange.

    
     

    TIM4->SR &= (~TIM_SR_UIF);
    TIM4->DIER |= TIM_DIER_UIE;
     Don't use RMW editing on SR registers. You don,t check if coresponding interrupt is enabled. 
     sign ~ should be before ( etc. 
     Mixing HAL and reg style is *****. 
    

    Walid FTITI_O
    Visitor II
    February 1, 2016
    arnold_w
    arnold_wAuthor
    Senior II
    February 1, 2016
    Posted on February 01, 2016 at 12:56

    Thank you for your replies. So, the problem was that I forgot to update the prescalar after it was set. The following code works great.

    void testTimer4(EventCallback_t timerInterruptCallback)

    {

    timerInterruptCallback_ = timerInterruptCallback;

    RCC->APB1ENR |= RCC_APB1ENR_TIM4EN;

    TIM4->PSC = 976;

    TIM4->EGR = TIM_EGR_UG; // Generate an update event to reload the Prescaler

    TIM4->ARR = 65505;

    TIM4->CNT = 0;

    TIM4->SR &= (~TIM_SR_UIF);

    TIM4->DIER |= TIM_DIER_UIE;

    HAL_NVIC_EnableIRQ(TIM4_IRQn);

    TIM4->CR1 |= TIM_CR1_CEN;

    }

    void TIM4_IRQHandler(void)

    {

    TIM4->SR &= (~TIM_SR_UIF);

    HAL_NVIC_DisableIRQ(TIM4_IRQn);

    TIM4->DIER &= (~TIM_DIER_UIE);

    TIM4->CR1 &= (~TIM_CR1_CEN);

    RCC->APB1ENR &= (~RCC_APB1ENR_TIM4EN);

    (void)timerInterruptCallback_((uint32_t)TIMER_4_EXPIRED, 0);

    }