cancel
Showing results for 
Search instead for 
Did you mean: 

Which interrupt for TIM1?

jamsoft
Associate II
Posted on June 06, 2013 at 20:48

Hello,

I've TIM1 set for PWM signal generation (STM32F407VG). Everything works well but I want an interrupt to be rised on the falling edge of pulse and I have no idea how to set it.

Currently I've the following settings for the TIM1 IRQ:

 

  NVIC_InitStructure.NVIC_IRQChannel = TIM1_CC_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

    

    //Attach_Tim_Interrupt(TIM1_IRQn, 0);

    TIM_ITConfig(TIM1, TIM_IT_CC1, ENABLE);

...

...

void TIM1_CC_IRQHandler(void) //Tim1 ISR

{

   TIM_ClearITPendingBit(TIM1, TIM_IT_CC1);

   ...

   ...

}

The interrupt function is rised (confirmed by breakponit) but I don't know if it is on the pulse rising edge, the falling edge or both of them.

I've found the following possible setting for the TIM1 interrupt:

NVIC_InitStructure.NVIC_IRQChannel =

  TIM1_CC_IRQn or

  TIM1_BRK_TIM9_IRQn or           

  TIM1_UP_TIM10_IRQn or

  TIM1_TRG_COM_TIM11_IRQn

and

TIM_ITConfig(TIM1, TIM_IT_CC1, ENABLE)

where

TIM_IT_CC1 can also stand for:

TIM_IT_CC2  or

TIM_IT_CC3 or

TIM_IT_CC4 or

TIM_IT_COM or

TIM_IT_Trigger  or

TIM_IT_Break or

TIM_IT_Update

Which settings should I use for the pulse falling edge interrupt?

Thank you in advance for any help...

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on June 07, 2013 at 11:36

Read the respective chapter in the User Manual first.

In the usual one-directional (upcounting or downcounting) mode, one edge of PWM is generated at the timer over/underflow (which corresponds to the Update Event (if not disabled)); the other at the respective Compare Event. Which edge is generated at which event depends on which PWM mode is chosen (and the direction of counting).

You are surely aware of the latencies associated with interrupts, are you.

JW

PS. You could try to ask also at some of the Czech-language fora, e.g. http://mcu.cz/plugins/smf/smf.php?board=531.0
jamsoft
Associate II
Posted on June 10, 2013 at 20:23

Hi Jan,

thank you for your answer - it was useful for me.

My problem is solved now :)

Thank you also for advice about the Czech forum :)