cancel
Showing results for 
Search instead for 
Did you mean: 

When will ST release STemWin 5.24?

Microstar
Associate III
Posted on May 07, 2014 at 16:23

It contains lots of new features.

#emwin #stm32
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on May 29, 2014 at 15:43

Hi,

We will use STemWin v5.24b starting from STM32CubeF4 V1.2.0 release planned early July.

With regards.

ezio
Associate
Posted on September 08, 2014 at 16:14

and when will 5.26 be released?

thanks,

ezio

Posted on September 09, 2014 at 18:27

Hi Ezio,

Till now, there is no official date of the STemWin 5.26 release.

Hope that can be released at the begining of next year (2015)

Regards.

frankv
Associate
Posted on March 06, 2015 at 23:48

Heisenberg,

I've been using STemWin1.1.2, which has emWin 5.22.  Is there any better information on an STemWin release that contains EmWinV 5.26?  

I need

 the function:   

LISTVIEW_EnableCellSelect().

Cheers,

Frank