2026-01-25 6:10 PM
Dear experts, why, under the same configuration for heterogeneous core communication, in the generated code, the debug section of the routine's initialization functions of IPPC and OPENAMP can be accessed, but the ones generated by ourselves cannot?
The following picture was generated by myself.
The following picture was generated by myself.
Why does the routine configuration add an extra "remote" and "setting" in the file attributes?
But there is none in the project that was generated by myself!
Seeking help online, dear experts!
2026-01-25 6:20 PM
Note: The second picture is an example screenshot from the process.