cancel
Showing results for 
Search instead for 
Did you mean: 

What Xferoption should be selected in SMBUS for restart condition?What is Xferoption for restart condition with change in direction(write to read)?

VKamb.1
Associate

/* List of XferOptions in usage of :

 * 1- Restart condition when direction change

 * 2- No Restart condition in other use cases

 */

#define SMBUS_FIRST_FRAME      SMBUS_SOFTEND_MODE

#define SMBUS_NEXT_FRAME     ((uint32_t(SMBUS_RELOAD_MODE|SMBUS_SOFTEND_MODE))

#define SMBUS_FIRST_AND_LAST_FRAME_NO_PEC     SMBUS_AUTOEND_MODE

#define SMBUS_LAST_FRAME_NO_PEC              SMBUS_AUTOEND_MODE

#define SMBUS_FIRST_FRAME_WITH_PEC (SMBUS_SOFTEND_MODE|SMBUS_SENDPEC_MODE))

#define SMBUS_FIRST_AND_LAST_FRAME_WITH_PEC   ((uint32_t)(SMBUS_AUTOEND_MODE | SMBUS_SENDPEC_MODE))

#define SMBUS_LAST_FRAME_WITH_PEC             ((uint32_t)(SMBUS_AUTOEND_MODE | SMBUS_SENDPEC_MODE))

/* List of XferOptions in usage of :

 * 1- Restart condition in all use cases (direction change or not)

 */

#define SMBUS_OTHER_FRAME_NO_PEC              (0x000000AAU)

#define SMBUS_OTHER_FRAME_WITH_PEC            (0x0000AA00U)

#define SMBUS_OTHER_AND_LAST_FRAME_NO_PEC     (0x00AA0000U)

#define SMBUS_OTHER_AND_LAST_FRAME_WITH_PEC   (0xAA000000U)

/**

From the above options in master mode which Xferotion should be selected if I want to generate a restart condition?

What is the difference between SMBUS_OTHER_FRAME_NO_PEC  and  SMBUS_FIRST_FRAME ?

I want to write a byte of data to slave with a restart condition by using HAL_SMBUS_Master_Transmit_IT(SMBUS_HandleTypeDef *hsmbus, uint16_t DevAddress, uint8_t *pData, uint16_t Size, uint32_t XferOptions)

and then receive data from slave using

HAL_SMBUS_Master_Receive_IT(SMBUS_HandleTypeDef *hsmbus, uint16_t DevAddress, uint8_t *pData, uint16_t Size, uint32_t XferOptions)

After receiving there should be a stop condition generated. So Xferoption while transmitting should be SMBUS_SOFTEND_MODE and while receiving it should be  SMBUS_AUTOEND_MODE. Please let me know if the procedure is correct?

But when should we call HAL_SMBUS_Master_Receive_IT()? Should I call it after the TC flag is set from the previous Transmission ie in (HAL_SMBUS_MasterTxCpltCallback()) or

While(1)

{

HAL_SMBUS_Master_Transmit_IT();

HAL_SMBUS_Master_Receive_IT();

}

should work?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0