2018-03-14 6:30 AM
Hi
We have an STM32L4x5 project. We are using
STM32CubeMX
to generate our HAL based framework and have a bunch of hardware all working great. We were noticing application level CRC errors on receipt of data being receiving via a CDC USB connection and this has caused me to create a simple test case which shows it. We are probably doing something wrong here, but would love some insight into this.char output[90] = ''0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567\r\n'';
int index = 0;
uint8_t * out = (uint8_t*)&output;
while (1)
{
USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData;
while (hcdc->TxState != 0){
// wait for usb tx done
}
if (CDC_Transmit_FS(out+index, 10)== USBD_OK)
{
index += 10;
}
if (index >= sizeof(output))
{
index = 0;
DelayMilliseconds(50);
}
WatchdogReset();
}
This is a complete 10 second hack of a test case which we put in main.c, but generates the same issue, which is on the PC we receive data like this:
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
01234567890123456789012301234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
01234567890123456789012345678901234567890123456789012301234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
0123456789012345678901234567890123456789012345678901234567890123456789012345678901234567
Here, we see an occasional duplicate DWORD. If we output a single byte at a time rather than 10, the issue occurs mode frequently.
If I add some debug output in the USB library where the data is being put onto the USB FIFO from our buffer pointers I see it being written correctly into the EP FIFO registers in order ok, but different data is being received.
Any hints as to what we're doing wrong here?
Oh yes, our functions for sending are:
static int8_t CDC_Init_FS(void)
{
/* USER CODE BEGIN 3 */
/* Set Application Buffers */
USBD_CDC_SetTxBuffer(&hUsbDeviceFS, UserTxBufferFS, 0);
USBD_CDC_SetRxBuffer(&hUsbDeviceFS, UserRxBufferFS);
FIFO_Init(&usbRxFifo, usbRxBuffer, USB_RX_BUFF_SIZE);
FIFO_Init(&usbTxFifo, usbTxBuffer, USB_TX_BUFF_SIZE);
usbLastTxLen = 0;
UplinkDecoderInit(&usbRxState);
state = 0;
return (USBD_OK);
/* USER CODE END 3 */
}
uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len)
{
uint8_t result = USBD_OK;
/* USER CODE BEGIN 7 */
USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData;
if (hcdc->TxState != 0){
return USBD_BUSY;
}
USBD_CDC_SetTxBuffer(&hUsbDeviceFS, Buf, Len);
result = USBD_CDC_TransmitPacket(&hUsbDeviceFS);
/* USER CODE END 7 */
return result;
}
Thanks, Dave
Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-03-14 5:59 PM
OTG_GUSBCFG
register reads as 00x40001840, so it has a value of 0xC for TRDT. Which looks ok according to table 307 which shows an AHB of 17.2 minimum for that value.2018-03-14 6:01 PM
Sorry, I already corrected my reply to myself.. it reads back as
0xC from the register.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.