cancel
Showing results for 
Search instead for 
Did you mean: 

Using Acoustic beam-forming, Acoustic source-localization for stm32f746

son1
Associate II
Posted on March 02, 2016 at 04:26

ST just introduces the library for beam-forming and sound source-localization.

However, they are applied for STM32 Nucleo board only (with node-locked library). I am using STM32F746 MCU, is there any way to use these LIBs in my MCU. 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on March 29, 2016 at 12:54

Hi phan.le_son,

In both UM1967 (Getting started with osxAcousticBF real-time beam forming software expansion for STM32Cube) and UM1968 (Getting started with osxAcousticSL real-time sound source localization software expansion for STM32Cube), it is said ''the library can be easily ported to any STM32F4 microcontroller with FPU unit.''.

So you have just to take into account hardware requirements and updates comparing your own board to the Nucleo one.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.